Mouser - White Papers

Battery Storage Meets Rising Grid Demand

Mouser Electronics White Papers

Issue link: https://resources.mouser.com/i/1526769

Contents of this Issue

Navigation

Page 4 of 5

Mouser Electronics White Paper As mentioned earlier, some automakers are also releasing EV charging electronics that can be tied to a home service, much like a backup generator. These systems can be used to charge the EV and supply the home with AC when the grid fails. In future cases, this vehicle-to-grid (V2G) connection may also use the EV battery as a full BESS—the EV battery used to reduce energy bills using smart control. Hence, smart homes with BESSs of the future may include solar or wind power, EV BESS, a home BESS, and the necessary systems to integrate these renewables and battery energy storage technologies in an optimized home energy system that minimizes home energy costs and ensures reliability even in severe weather or outages. To achieve this, however, designs will need to achieve high levels of efficiency, reliability, and performance while mitigating environmental challenges such as temperature extremes, high winds, moisture ingress, pests, and corrosives. Designers must protect these electronics from the ambient environment while ensuring an optimal local environment for the electronics. For these reasons, home BESSs and other home energy electronics must be located within protective enclosures that often include thermal management solutions. Within these enclosures, there are a variety of interconnect types. These include terminal blocks, many types of electrical wiring, varieties of connector types, and busbars. There are also several types of interconnects and conduits used to connect the different home energy electronics enclosures. Designers must select these interconnects to conform to regional building codes and to ensure the safety and performance of these systems. In addition to reliability, interconnect considerations must also account for the interconnect adding resistance, inductance, and capacitance, which may be affected by environmental conditions and could impact the operation of the electronics in the system. As shown in Figure 4, the typical connector requirements for a BESS include the following: 1. SW1 Connectors 2. Terminal Blocks 3. Mini-Fit Connectors 4. Off-the-Shelf Power and Signal Discrete Wire Cable Assemblies 5. Nano-Fit Connectors 6. Busbars 7. PowerPlane Busbar Connectors 8. Mega-Fit Connectors Figure 4: Typical connector requirements for a BESS. (Source: Molex)

Articles in this issue

Links on this page

view archives of Mouser - White Papers - Battery Storage Meets Rising Grid Demand