Supplier eBooks

The RF Design Handbook: Theory, Components, and Applications

Issue link: https://resources.mouser.com/i/1541351

Contents of this Issue

Navigation

Page 32 of 61

| 32 the dielectric, L' is the inductance per unit length, and C' is the capacitance per unit length. η π μ π πϵ In an ideal coaxial cable, the electromagnetic fields propagate in TEM mode, meaning electric and magnetic fields are perpendicular to each other and the direction of travel. However, at higher frequencies, additional modes (like TE11) start to appear, impacting signal integrity. It is also possible to estimate the loss per unit length of a coaxial transmission line using the ohmic and dielectric losses of the conductors and dielectrics used in the coaxial line construction. The following equation—where is the attenuation per unit length, c is the ohmic losses of the conductors, d is the dielectric losses, R s is the resistivity of the conductors, and tan is the loss tangent of the dielectric—shows that the attenuation of a coaxial line is greater for smaller dimensions of a and b. α α α η ω δ Coaxial cables are broadband interconnects, which can operate down to DC (0Hz). However, their upper cutoff frequency is determined by their physical geometry, as higher frequencies can introduce additional propagation modes beyond the fundamental TEM mode. Specifically for coax, the TE11 mode begins to propagate above a certain cutoff frequency and is approximated by the following equation, where f c is the cutoff frequency, c is the speed of light, λ c is the cutoff wavelength, a and b are dimensions of the transmission line, μ r is the relative permeability, and ε r is the relative permittivity: λ π μ ϵ If modes other than TEM are operating within the transmission lines, the reflections of the higher-order modes can cause interference, increase loss, and reduce the transmission line's voltage standing wave ratio (VSWR) performance. Larger coaxial cables have a lower cutoff frequency but can handle higher voltages and power while exhibiting lower attenuation per unit length compared to smaller coaxial cables. ADL8113 Low Noise Amplifier mouser.com/adi-adl8113-low-noise-amp

Articles in this issue

Links on this page

view archives of Supplier eBooks - The RF Design Handbook: Theory, Components, and Applications