Mouser Electronics White Papers
Issue link: https://resources.mouser.com/i/1542976
Mouser Electronics White Paper When designing for these diverse applications, engineers must consider factors such as antenna size, beamforming, and power management, which drive performance in modern radar and communication systems. Commercial and Civil Applications Remote sensing satellites acquire critical data about the Earth's surface and atmosphere using passive or active methods. Passive satellites detect natural energy, such as sunlight reflecting off the Earth's surface, while active satellites emit their own signals and measure the energy reflected back to them. Both active and passive remote sensing satellites rely on several frequency bands for sensor transmissions, with X-band being an ideal choice for urban and weather monitoring applications. With shorter wavelengths and higher resolution, the X-band supports a variety of civil and commercial systems that require accurate, real-time imaging. Such systems rely on a band's capacity to maintain signal integrity in rain, fog, and other adverse conditions, while providing detailed surface and target information. Weather Radar X-band wavelengths provide sufficient resolution to identify precipitation, making X-band radar a valuable tool for weather monitoring and forecasting. The hardware is small enough to fit on mobile X-band weather radar systems, which can be deployed in areas of interest or where mountainous terrain blocks satellite signals. These mobile systems provide high-resolution local data for real-time storm tracking and improved regional forecasts. Infrastructure Protection With modules light enough for air and space travel, X-band radar makes an excellent tool for surveying land and infrastructure. The high-resolution signals can create detailed topographical maps (Figure 1) and monitor buildings and vegetation for subtle changes that may indicate maintenance is required. The combination of X-band synthetic aperture radar (SAR) and the Permanent Scatterer Interferometry SAR (PS-InSAR) technique—a remote sensing method that employs multiple SAR images of the same area to measure changes—enables the detection of millimeter-scale ground deformations. 2 Figure 1: Topographical relief image of Patagonia from the US National Aeronautics and Space Administration (NASA) Shuttle Radar Topography Mission, which featured the Spaceborne Imaging Radar-C/X-Band Synthetic Aperture Radar (SIR-C/X-SAR) instrument. (Source: NASA/JPL/NIMA) 3 For ground observation applications, the revisit interval is an important figure of merit. The revisit interval is the time it takes a satellite to fly over the same spot again and is a function of the latitude of the area under observation, the satellite's orbit path, and the number of satellites in a constellation. Leading earth- monitoring solutions have revisit intervals measured in hours, providing near-real-time monitoring of structures and landmasses. Air Traffic Control Air traffic control systems use phased-array X-band radar antennas for accurate aircraft tracking and fast update cycles. The shorter wavelength supports accurate position detection and can separate multiple aircraft flying close together, even in heavy rain. With smaller antennas and higher angular resolution, X-band radar provides the data density needed for reliable short- and mid-range coverage in commercial and defense aviation. Marine Radar The X-band is also used in marine and aviation radar systems for navigation, collision avoidance, weather monitoring, and traffic control. International maritime safety regulations defined by the Safety of Life at Sea (SOLAS) convention require X-band radar on vessels weighing over 300 tons. 4 As sudden weather changes and harsh sailing conditions are common on sea and ocean voyages, X-band systems excel in diverse weather conditions. The compact antenna size required for X-band operation makes these systems suitable for deployment on vessels with limited space.