Mouser - White Papers

Advanced Cooling and Power Solutions for High-Density AI Data Centers

Mouser Electronics White Papers

Issue link: https://resources.mouser.com/i/1543982

Contents of this Issue

Navigation

Page 2 of 4

Mouser Electronics White Paper become evident. Air has a low specific heat capacity, so removing higher thermal loads requires higher airflow velocity; however, higher fan speeds increase energy consumption and acoustic noise. On top of this, the tightly packed arrangements of AI servers further reduce efficiency by restricting flow paths. The term liquid cooling may evoke images of equipment completely submerged in fluid, but this is only one type of liquid cooling, known as immersion cooling, and it supports extremely high densities. With the right preparation, servers can operate fully submerged in a dielectric liquid that transfers heat directly to an external heat exchanger. But immersion cooling requires infrastructure planning. Facilities must be built to support fluid containment, handling, and long-term maintenance. Retrofitting existing installations can be complex. For greenfield sites designed around immersion from the outset, this liquid cooling method can support long-term thermal objectives. However, for many operators, incremental alternatives offer a more practical starting point. Liquid cooling does not require the submersion of hardware. Rear door heat exchangers represent a more easily adopted transition. Installed on the back of a rack, they capture hot exhaust air before it disperses into the server room. A liquid loop within the door extracts heat via an integrated exchanger, reducing the need for room-level cooling without redesigning internal server layouts. An advantage of this approach is that operators can deploy it selectively on high-density racks. Direct-to-chip cooling is an even more focused liquid cooling approach. Cold plates mount directly onto processors or accelerators, and coolant flows through internal channels within the plate to remove heat at its source (Figure 1). This technique reduces dependence on large heatsinks and high-speed fans. Moreover, the space created within the server becomes available for additional compute modules or improved airflow management for the remaining components. Figure 1: Direct-to-chip liquid cooling architecture showing rack-level manifolds supplying cold plates within dense server configurations. (Source: Amphenol LTW)

Articles in this issue

Links on this page

view archives of Mouser - White Papers - Advanced Cooling and Power Solutions for High-Density AI Data Centers