Skip to main content

Micropower MEMS Accelerometers Advance Smart Agriculture Monitoring

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

Published June 2, 2026

The agriculture industry faces increasing pressure to maximize yields while monitoring animal welfare with minimal human intervention. This demand has led to the proliferation of smart farming, which relies heavily on remote edge nodes to track livestock health, monitor equipment condition, and optimize resource allocation. Deploying these sensor networks significantly reduces the need for manual oversight across vast agricultural landscapes. To achieve this operational scale, engineers must design battery-powered devices capable of surviving autonomously for years in harsh, remote locations. Balancing the demand for continuous, high-resolution physical data with severe energy constraints presents a complex design challenge.

This week's New Tech Tuesdays explores how continuous motion sensing and ultra-low-power acceleration measurement bring vital edge intelligence to modern agricultural environments.

The Need for Always-On Sensing in Agriculture

Livestock tracking collars and ear tags require batteries that last multiple years to avoid the labor-intensive process of replacing power sources. These edge nodes monitor step counts, resting periods, and erratic movements to help infer changes in animal health, feeding habits, and reproductive cycles. However, achieving continuous motion detection quickly drains batteries in traditional sensor architectures. Engineers face the constant challenge of balancing real-time monitoring requirements with strict energy budgets. Sending continuous raw data streams over wireless protocols quickly depletes small batteries. Instead, modern designs require the sensor node itself to possess sufficient local intelligence to filter mechanical noise and detect specific motion signatures.

Addressing the Power and Processing Dilemma

Solving the power consumption dilemma requires a fundamental shift from power-hungry continuous polling to intelligent, event-driven architectures. Instead of the main embedded processor waking up frequently to interrogate the accelerometer, the sensor must autonomously handle initial data gathering. By implementing deeply embedded first-in, first-out (FIFO) buffers, sensors collect and store substantial acceleration data locally. The sensor wakes the host processor only when the buffer reaches a specific watermark or when a predefined motion threshold is exceeded. Processing step counts and activity thresholds directly on the sensor die dramatically reduces host wake time and allows firmware to transmit compact event summaries instead of continuous raw acceleration streams. By lessening overall microcontroller active time, this localized processing architecture extends the operational life of the entire smart agriculture system.

Optimizing Sensor Architectures for the Edge

Designing edge nodes for remote deployment requires optimizing signal integrity without increasing power consumption. A 3-axis microelectromechanical system (MEMS) accelerometer must operate across varying voltage ranges to support the natural discharge curve of coin-cell batteries over time. Noise density and sensitivity remain critical specifications for these condition-based monitoring applications. Sensors must accurately differentiate between subtle physiological movements of livestock and ambient environmental vibrations, such as wind or heavy machinery. Internal multi-pole anti-aliasing filters help condition the raw signal before digitization, ensuring the microcontroller receives clean, actionable data. Furthermore, flexible interrupt routing becomes essential in these power-constrained environments. Advanced sensor designs feature dual interrupt pins, allowing engineers to map specific mechanical events—such as a sudden impact or continuous inactivity—to distinct hardware wake states.

The Newest Products for Your Newest Designs®

The ADXL366 micropower 3-axis MEMS accelerometer from Analog Devices offers exceptional efficiency for condition-based monitoring designs. Operating on a flexible supply range of 1.1V to 3.6V, the ADXL366 consumes a mere 0.96µA at a 100Hz output data rate and drops to 47nA in standby mode. This ultra-low-power profile enables agricultural sensors to operate for years from a single coin-cell battery.

The ADXL366 integrates a dedicated step counter that draws only 120nA, making the device ideal for continuous livestock-tracking applications. Single-tap and double-tap detection adds only 35nA of current. A deep 512-sample embedded FIFO buffer minimizes the host processor load by locally storing multi-axis acceleration data. Engineers can leverage adjustable threshold sleep and wake-up modes to enable autonomous motion-activation, extending battery life across remote agricultural deployments. Featuring a high sensitivity of 0.25mg/LSB and an internal multi-pole anti-aliasing filter, the ADXL366 delivers the precise, low-noise measurements required for critical edge intelligence.

Tuesday’s Takeaway

Continuous motion sensing and ultra-low-power acceleration measurement bring vital edge intelligence to modern agricultural environments. By integrating intelligent features like step counting, local FIFO buffering, and autonomous hardware interrupts, advanced MEMS accelerometers enable continuous monitoring without sacrificing battery life. Moving preprocessing tasks directly to the sensor node alleviates the burden on the host microcontroller and reduces power-heavy wireless transmissions. Smart agriculture operations ultimately gain actionable, real-time insights that improve animal welfare, optimize farm productivity, and ensure long-term system reliability.

About the Author

Mouser, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.

Profile Photo of Mouser Technical Content Staff