Supplier eBooks

Qorvo - Next-Gen Wi-Fi Applications and Solutions

Issue link: https://resources.mouser.com/i/1313794

Contents of this Issue

Navigation

Page 26 of 27

27 Qorvo 2020 Figure 1 Packing multiple high-performance RF front-end filters in smaller space while improving performance lets hexaplexers such as this multiband filter provide superior performance in smaller designs Improving Performance Through Precision Filitering Key to improving performance are filters, but older space- eating Surface Accoustic Wave (SAW) filter technologies are reaching a brick wall as far as being effective solutions to the doubling of RF bands we will see in the near future. Supplanting SAW filters is BAW technology. This technology can handle higher power levels than surface accoustic wave devices. Electric current distrubutes more freely and there are no narrow channels of fingers prone to electromigration damage as in SAW filters. Bulk filters have been used to partition the bands and are proving a more reliable bandwidth within band. Bulk Accoustic Wave technology extends the edges of the filters while maintaining sharp band edges. SAW and BAW filters are forms of electromechanical resonators. Bulk Accoustic Wave filters, which can be made using crystal quartz, can be 1,000 times smaller than ceramic technologies while retaining low cost at high- volume manfacturing. As this technology supplants older Surface Accoutstic Wave solutions, the tightly packed bulk filters can allow smaller, more clever use of specific bands and power levels to set up a next-generation band-sharing technique. New Ways of Partitioning With more filters exhibiting higher power levels taking up less space, device-specific, and even protocol-specific partitioning of the air waves can take place. Additionally, design engineers can classify power levels of criticality, throughput, or other importance so that channel assignments for noncritical transmissions avoid these channels. For example, a high-speed streaming multimedia link has higher bandwidth needs than SMS texting services. An interruption in the streaming could be a turnoff if not enough bandwidth or buffering is used. Seconds of delay in SMS services would not even be noticed. By the same token, newly emerging medical devices connected to the Internet of Things could use specific subsets of the newly evolved bandwidth to assure the most reliability while monitoring a patient, or transferring error- free vitals. Even assigned fallback channels can be used to increase reliability. Where to Begin Those pioneering the technology usually have a lot to say. In this case, check out what Qorvo is introducing. Qorvo BAW filters range from 1.5GHz to 9GHz, encompassing the consumer wireless bands as well as carrier services. Parts such as the QPQ1909SR perform signal-conditioning filtration within the 2402MHz to 2494MHz bands for Wi-Fi bandage (Figure 1). Terminating into 50Ω, the low 0.8db to 1.2db insertion loss is important for maintaining signal integrity. But while many are unfamiliar with how to design with BAW, aids are available to guide you through the journey. Take for example the QPQ1909EVB01 Active Filter Development Tools Evaluation Board Kit. This uses the high-performance, high-power edgeBoost™ Wi-Fi technology for channels 1 through 14. This means end users will see a better quality of service as well as higher regulatory power allowances (to +30dBm averaged input power). Note how the higher performance channels in conjunction with a priority scheme can ensure more reliable data communications to more critical applications. And don't just think of BAW as a better Wi-Fi solution. Other BAW technologies from Qorvo are useful for GPS, diplexers, duplexers, and other assorted protocol-specific access points, routers, gateways, and wearables. If you are going to filter, do it in bulk. Conclusion With the introduction of next-generation services and devices, more frequencies, bandwidth, coexistence, and interference immunity are required. As a result, design engineers must maximize spectrum utilization. BAW technology and filters enable the partitioning of frequency bands for more precision filtering to capture stronger and more reliable signals with enhanced noise immunity.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Qorvo - Next-Gen Wi-Fi Applications and Solutions