Supplier eBooks

Littlefuse - Circuit Protection for High-Speed Serial Interfaces

Issue link: https://resources.mouser.com/i/1437732

Contents of this Issue

Navigation

Page 12 of 33

13 littelfuse.com V Each line of the USB-C port requires optimized circuit protection. To investigate, let's start at the bottom of the table in Figure 2, at Roman numeral five (V) and work our way up. One first notices an ESD protector for the USB-C port's power lines. Each V bus power line could provide power at voltages up to 20V. Typical ESD devices are only capable of withstanding 5V, 6V, or even 12V of sustained power. Littelfuse SPHV24 Series is designed to handle 20V without clamping. When an ESD event comes in, it can accurately protect against that event. Figure 3: Circuit protection solutions for USB 3.0 (Source: Littelfuse) IV IV indicates protection for the CC line and the SBU lines. Since the data rate on these lines are fast but not as fast as the SuperSpeed lines, the capacitance of an ESD protector can be a little higher. For data speeding, capacitance, and the relationship, the faster your data speed, the lower one wants capacitance. This is because capacitance can degrade the signal to a point where it attenuates, and it's unreadable by the device receiving it. So on this line, because it's lower speed, a higher capacitance device can be used and typically is lower in price. Littelfuse would suggest something such as the SP1006 Series single-channel device. III The SuperSpeed lines carry data at extremely fast data rates. Up to eight of these could be in action at any one point in time. Signals with faster data speeds are more sensitive to interference caused by the capacitance of components connected to them. Due to the number of data lines and very fast data speed associated with the SuperSpeed lines, ESD protection, such as the SP3213 Series, must be very small and have extremely low capacitance so that it fits within the allotted space and does not interfere with the data signal. Figure 2: Circuit protection solution for USB Type-C (Source: Littelfuse)

Articles in this issue

Links on this page

view archives of Supplier eBooks - Littlefuse - Circuit Protection for High-Speed Serial Interfaces