Supplier eBooks

Renesas - 7 Experts on Brushless DC Motor Control

Issue link: https://resources.mouser.com/i/1437741

Contents of this Issue

Navigation

Page 10 of 25

11 Chapter Two: Motor Controllers and Drivers end. In BLDC motors, the front end includes filtering capacitors to convert input voltage to a suitable internal DC voltage. In BLDC motors that use position sensors to identify the rotor position, the front end also includes inputs for the sensors. The digital back end includes the following components: • A microcontroller provides motor starting and control functions. Here, the more sophisticated the control requirements, the larger the algorithms and the more processing power you need. • Pulse width modulation (PWM) circuitry modulates motor speed by regulating the driving voltage pulse width. The PWM circuitry keeps the output voltage at the rated voltage irrespective of load. • Power drivers provide the power necessary to operate the BLDC motor's functions. BLDC Drivers BLDC drivers are bridges between the controller and the motor that provide power for the motor to function. These "power amplifiers" use the low power input from the controller to produce more current and higher voltages than can be realized using a microcontroller pin. "Digital control allows for easy and flexible implementation of the control." Dr. Naveed-ur-Rehman Malik Motor Drives Engineer, Dyson Designers are driving up to three BLDC motors with just one controller. This is a huge benefit in that you need just one microcontroller unit, you do not have to deal with serial communication across motors, and yet you still have the benefits of multiple motors. Miguel Mendoza Principal Technical Marketing Manager, Renesas Electronics

Articles in this issue

view archives of Supplier eBooks - Renesas - 7 Experts on Brushless DC Motor Control