Supplier eBooks

ROHM - Driving the Future of Automotive Solutions

Issue link: https://resources.mouser.com/i/1437744

Contents of this Issue

Navigation

Page 10 of 36

BD183x7EFV Advantage | Energy Sharing Function with External Resistors Rather than dissipating all of the LED power in the driver IC, as competitor devices do, ROHM's new products include a pin that allows the power to be dissipated in the external thermal resistors. So, instead of requiring two driver ICs to reduce the power dissipated in each, these external power resistors reduce the design's size and cost ROHM Company A Company B Total BOM 0 pcs compared to Company A -7 pcs compared to Company B Total Area -30.1% compared to Company A -50.0% compared to Company B image of the area size Figure 4: Example of BOM and Board Space Savings with BD183x7EFV The PBUS function reduces the need for additional control circuitry by integrating the control function between multiple driver ICs to turn off all LEDs when an open or short is detected on any LED channel. This function is currently required in automobiles in the European Union, and it can be accomplished without additional components when using a BD183x7EFV driver IC. VINRES VIN CRT GND OUT1 OUT2 OUT3 OUT4 SET1 SET2 SET3 SET4 DISC MSET1 MSET2 PBUS VINRES VIN CRT GND OUT1 OUT2 OUT3 OUT4 SET1 SET2 SET3 SET4 DISC MSET1 MSET2 PBUS VINRES VIN CRT GND OUT1 OUT2 OUT3 OUT4 SET1 SET2 SET3 SET4 DISC MSET1 MSET2 PBUS BD18337EFV-M BD18347EFV-M U1 BD18337EFV-M BD18347EFV-M U1 BD18337EFV-M BD18347EFV-M U1 LED ON LED OFF LED OFF 1 OUT all OUT when IC detect LED open/short Figure 5: PBUS Function BD183x7EFV Advantage | PBUS Function 7

Articles in this issue

view archives of Supplier eBooks - ROHM - Driving the Future of Automotive Solutions