Supplier eBooks

ROHM - Driving the Future of Automotive Solutions

Issue link: https://resources.mouser.com/i/1437744

Contents of this Issue

Navigation

Page 27 of 36

Solving the Challenges of Driving SiC MOSFETs with New Packaging Silicon carbide (SiC) MOSFETs offer tremendous new characteristics and capabilities, but they also present new challenges. ROHM semiconductor devices allow engineers to take full advantage of SiC MOSFETs while also overcoming the challenges of driving them. Transistors are sometimes thought of as the building blocks of digital electronics. The invention of the semiconductor-based transistor, replacing the vacuum tube for electrical switching, enabled some of humankind's greatest tech- nology leaps. The most common transistor type in electronics is the metal oxide semiconductor field-effect transistor Figure 1: Semiconductor material comparisons (Silicon Carbide vs. Silicon vs. Gallium Nitride) 24 expanding the Capabilities of moSFets (MOSFET). These transistors take advantage of semiconductor materials' peculiar properties to allow small electrical current signals to control the switching of sometimes much larger current signals. One type of MOSFET is used as a switch in power electronics circuits, and it is specially optimized to withstand high voltages and pass load current with minimal energy loss. A new extremely hard compound semiconductor material, silicon carbide, provides a number of advantages over silicon for making these power-switching MOSFETs. SiC has 10x the breakdown electric field strength, 3x the bandgap, and enables a wider range of p- and n-type control required for device construction. SiC also has 3x the thermal conductivity, meaning 3x silicon's cooling capability.

Articles in this issue

view archives of Supplier eBooks - ROHM - Driving the Future of Automotive Solutions