Supplier eBooks

Xilinx - Programmable Single-Chip Adaptable Radio Platform

Issue link: https://resources.mouser.com/i/1437750

Contents of this Issue

Navigation

Page 15 of 27

Xilinx PRODUCT SPOTLIGHT UNBOXING THE ZYNQ ® ULTRASCALE+ ™ ZCU111 EVALUATION KIT s | 4 | | 16 | RF-DAC Unlike the ADC, the DAC has only one title type. This contains quad RF-DACs, and a phase-locked loop to provide a common clock to all converters within the tile. Like the ADC tile, the RF-DACs can be configured for a real output individually or paired to provide an I/Q output capability. Another difference with the RF-ADC tile is the RF-DAC analog outputs. Unlike the RF-ADC inputs, which are voltage-driven, the RF-DAC outputs are differential current buffers. This differential output can also be AC coupled using capacitors or DC coupled. The output current is configurable to be either 20mA or 32mA. The termination voltage supplied will change depending upon the current required. Clocking & Synchronization One of the more complex issues in RF signal processing is the distribution of the clocking network. Each tile provides a differential clock input within the RFSoC. This clock can be used to clock the RF-ADC or RF-DAC directly, or it can be connected straight to the tile PLL to generate the required sampling frequency. To assist with synchronization, each RFSoC also provides an SYSREF pin pair. This can be used to enable multiple tiles and multiple device synchronizations if required. The synchronization between tile and devices uses a simplified version of JESD204B SYSREF, which is popular to synchronize discrete devices. Multi-Nyquist Operation Data converters used in the RFSoC ADC and DAC tiles are designed to operate across both the first and second Nyquist zones. The first Nyquist zone is where signals Xilinx Zynq ® UltraScale+ ™ MPSoC ZCU104 Evaluation Kit Xilinx Zynq ® UltraScale+ ™ MPSoC ZCU106 Evaluation Kit Learn more > Learn more > fall between 0 and Fs/2, while the second Nyquist zone falls between Fs/2 and Fs. By careful selection of the numerically controlled oscillator, it is possible to down- convert from higher Nyquist zones provided the full bandwidth is supported. When working with the RF-DAC, it is also possible to use the NCO to provide up-conversion and work across the first and second Nyquist zones. To support this, the RF-DAC enables the use of a mix-mode output to increase the power available. Learn more > Learn more >

Articles in this issue

Links on this page

view archives of Supplier eBooks - Xilinx - Programmable Single-Chip Adaptable Radio Platform