Supplier eBooks

Silabs - Connectivity for Building Home Automation

Issue link: https://resources.mouser.com/i/1442793

Contents of this Issue

Navigation

Page 5 of 21

6 Bluetooth 5 – Now with Mesh Range, speed, and bandwidth are the core improvements introduced in Bluetooth 5. Doubling the speed and quadrupling the range of Bluetooth 4, Bluetooth 5 has added many additional improvements over previous versions. Data length extensions (DLE) allow for eight times the previous message length. These new enhancements of Bluetooth 5.0 focus on increasing functionality for home automation and the IoT. Two new features for Bluetooth 5 deserve a closer look: Mesh networking and beaconing. Mesh networking is something new for Bluetooth. Considered a drawback in previous versions, each node of the network could only communicate with the hub in a star-like relationship shown (Figure 3). Bluetooth 5 has incorporated mesh networking, which allows node-to-node communication. Aside from the improvements in speed that Bluetooth 5 gives home automation components, it's worth noting that wearables will benefit from the increased data rate and range. I've owned two trackers/wearables, and my biggest disappointment with both was battery life. Wearable devices typically operate in a low-power sleep mode. When needed, they quickly wake, send or receive data, and then go back to sleep mode to save power. Since the data rate of Bluetooth 5 is faster, transmission time is shorter, thus saving power. Beacons are a new feature of Bluetooth 5 that very effectively broadcast short messages over short distances and track Bluetooth-enabled devices without the need for pairing between the beacon and the device. Although the retail industry is the current focus of beaconing, home and industrial applications are soon likely to take advantage of the very low power consumption of the beacon. Several companies have already started producing Bluetooth 5 supported systems on a chip. The Silicon Labs EFR32MG13 Mighty Gecko Multi-Protocol can be used for battery-operated applications and other systems requiring high-performance and low-energy consumption. This System-on-a-Chip (SoC) is designed for home automation and other IoT applications: - IoT multi-protocol devices - Connected home - Lighting - Health and wellness - Metering - Home and building automation and security Figure 4: The Silicon Labs EFR32MG13 Mighty Gecko Multi-Protocol. Source: Mouser Electronics Silicon Labs BGM13P Blue Gecko Bluetooth Mesh Modules offer a turnkey SoC Bluetooth 5 system in a compact package. Focused even more on Bluetooth 5 mesh systems, its applications include: - IoT end devices and gateways - Wearables - Health, sports, and wellness devices - Industrial, home, and building automation - Smartphone, tablet, and PC accessories - Beacons Figure 3: Illustration of hub and spoke, or "star," network and a mesh network layout. Figure 5: The Silicon Labs BGM13P Blue Gecko Bluetooth Mesh Modules. Source: Mouser Electronics

Articles in this issue

Links on this page

view archives of Supplier eBooks - Silabs - Connectivity for Building Home Automation