Supplier eBooks

Silabs - Connectivity for Building Home Automation

Issue link: https://resources.mouser.com/i/1442793

Contents of this Issue

Navigation

Page 6 of 21

7 Bluetooth 5 vs. Zigbee 3.0—How Do Home Automation Features Stack Up? The table below represents a head-to-head comparison of Zigbee 3.0 and Bluetooth 5 home automation features. Data for this and the following table was presented in a Mouser-sponsored webinar in April 2017. The cells marked in red show an advantage of one protocol over another. As shown, Bluetooth 5 has the specification advantage when compared head to head. But, the fact that Bluetooth 5 is still relatively new requires some caution in predicting performance in the medium-to-long term. That said, head-to-head, it looks like Bluetooth 5 is the performance winner. Though home automation is currently in the spotlight, the real jackpot for IoT and mesh networked communications is the Industrial IoT (IIoT). Industrial and commercial automation applications can take advantage of performance advances in Bluetooth 5, Zigbee 3.0, and other protocols. Table 2: How Industrial IoT (IIoT) Needs are Different from Consumer IoT Commercial building and factory automation represent major new markets for low-power mesh networks. These segments demand heavy-duty, industrial-grade solutions and have tight reliability, scalability, and security requirements that Bluetooth mesh in particular seems positioned to deliver. Zigbee 3.0 Bluetooth 5 Power Consumption Moderate Very low Battery Life 2 years (More with Green Power) Up to 10 years Maximum Range (indoor) 92m 182m Maximum Data Transfer Rate 250kbps 2000kbps Overall Cost Moderate Low Industry Support Growing Ubiquitous/everywhere Industrial Devices Consumer Devices Battery Life Up to 10 years Several days Connectivity Wide Limited Hardware Life Possibly decades A few years Cloud Integration Possible Extensive Security Critical Important Reliability Essential Important Data Extensive Minor Beaconing Vast Minimal Table 1: Zigbee 3.0 vs. Bluetooth 5 Specifications Compared

Articles in this issue

Links on this page

view archives of Supplier eBooks - Silabs - Connectivity for Building Home Automation