Supplier eBooks

Bourns - Electrification of the Vehicle

Issue link: https://resources.mouser.com/i/1442820

Contents of this Issue

Navigation

Page 18 of 23

being measured. A 40mA BCI test level is sufficient for most industrial applications. The 200mA test level is typically used for automotive testing. The Bourns® Model SM91501AL and SM91502AL have been evaluated by certain BMS IC manufacturers for select automotive applications and have successfully passed requirements for BCI. Summary and Conclusions The demand for Li-ion battery power is predicted to grow at a CAGR of 20-30 percent over the next eight years. Battery Management Systems that integrate isolated communications are expected to be an important part of the safety and security of the battery system. An effective and reliable BMS will help increase the lifespan of Li-ion cells while also enhancing safe operation for end users. Offering an optimal protection solution for isolated communications in industrial and consumer BMS applications, Bourns engineered its latest Model SM91501AL and SM91502AL BMS transformers with the higher working voltages of 1600V and 1000V, respectively. They feature an inductance value of 150µH and 450µH over an operating temperature range of -40˚C to + 125˚C which meets higher voltage BMS requirements. Additionally, the transformer windings use fully insulated wire passing the dielectric strength (Hi-POT) test, further increasing electrical insulation protection for overvoltage transients. Bourns ® Model SM91501AL and SM91502AL have been tested by several BMS IC companies in their test laboratories who found them to function well with their chipsets, passing the necessary BCI tests. | 19 | Key Features: • -40°C to +85°C operating temperature range • 0.085Ω to 8.500Ω R1 maximum resistance • 6V to 30V maximum voltage Key Features: • -40°C to +125°C operating temperature • Hi-Pot Isolation Voltage: 4300VDC • Includes common mode chokes for noise rejection Key Features: • Fast tripping resettable circuit protection • 0.05A to 1.75A hold current • 0.090Ω to 50.000Ω R1 maximum resistance MF-NSMF Multifuse ® AEC-Q200 Compliant PTC Resettable Fuses BMS Signal Transformers MF-USMF Multifuse ® AEC-Q200 Compliant PTC Resettable Fuses mouser.com/new/bourns/bourns-mf-nsmf/ mouser.com/new/bourns/bourns-bms-transformers/ mouser.com/new/bourns/bourns-mf-usmf/

Articles in this issue

Links on this page

view archives of Supplier eBooks - Bourns - Electrification of the Vehicle