Supplier eBooks

NXP - Imagine the Possibilities

Issue link: https://resources.mouser.com/i/1442826

Contents of this Issue

Navigation

Page 12 of 27

AI SBC-S32V234 • S32V234 Processor with Linux BSP for SBC-S32V234 • Video input (2 x MIPI-CSI2) • Video Output (RGB to HDMI converter) LEARN MOREu Let's remind ourselves of the five (5) levels of automated driving as outlined by SAE International standard J3016: Level 1: Driver Assistance – The vehicle provides a specific function, such as speed control or steering Level 2: Partial Automation – The vehicle assists in functions like steering, acceleration, and braking Level 3: Conditional Automation – The vehicle can drive itself, but the driver has to monitor and be able to take over at any time Level 4: High Automation – The vehicle can take over driving on surface streets, but not highways or freeways Level 5: Full Automation – The vehicle takes over driving altogether, allowing drivers to remain in a "mind-off" state To accelerate the development and deployment of Level 3 automated drive capabilities and beyond, automotive stakeholders will need functions such as Driver Monitoring Systems (DMS), Pedestrian Detection, Lane Keep/Assist, Traffic Sign Recognition, Collision warning, and avoidance and blind-spot monitoring. Over time, all of these systems may be necessary to comply with NCAP safety standards. Automotive engineers will need to develop their applications with a processor that has automotive-grade reliability, functional safety, and security capabilities. The NXP S32V vision processor provides just that, along with the NXP S32V PROCESSOR FOR VISION AND MACHINE LEARNING APPLICATIONS 13

Articles in this issue

Links on this page

view archives of Supplier eBooks - NXP - Imagine the Possibilities