Supplier eBooks

Qorvo - Powering Up Your Design

Issue link: https://resources.mouser.com/i/1442844

Contents of this Issue

Navigation

Page 11 of 31

12 Powering Up Your Design Figure 7: Using the ACT88329EVK1-101 Evaluation Kit to exercise the ACT88329 PMIC requires standard bench instrumentation as well as a kit-supplied USB-to-I2C interface dongle. (Source: Qorvo).. ACT88329 Advanced Power Management ICs (PMIC) LEARN MORE > ACT88329EVK1-101 Evaluation Kit LEARN MORE > Configuring this versatile, flexible device involves examining and characterizing multiple parameters. The task is greatly simplified by the corresponding ACT88329EVK1-101 Evaluation Kit (Figure 7). Using this kit requires just a few standard engineering items. (If you don't have an electronic load, the power level is low enough—on the order of a few tens of watts—that a traditional resistive load can be used, but the e-load is much more versatile). All that is required are the following: A supplied USB-to-I 2 C "dongle" Power supply (3.3V/4A for full-power operation) Oscilloscope (100MHz, two channels) Loads, electronic or resistive (3A minimum-current capability) Digital multimeters (DMM) Windows-compatible computer with available USB port The PC-based GUI begins with a basic mode that allows the user to easily change one or more IC settings (Figure 8). The basic mode is followed by an advanced mode that lets designers see all available user-programmable options (Figure 9). Configuring this versatile, flexible device involves examining and characterizing multiple parameters.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Qorvo - Powering Up Your Design