Supplier eBooks

Bourns - Achieving Enhanced Performance and Reliability

Issue link: https://resources.mouser.com/i/1442856

Contents of this Issue

Navigation

Page 25 of 27

| 26 | Recommendations for Signal Processing Bourns developed the typical current source module block diagram, shown in Figure 2, to evaluate a shunt-based current measurement system's accuracy. The module consists of an Analog Front End (AFE) with a current sense amplifier with analog buffer, 24-bit ADC and Serial Peripheral Interface (SPI). There are several high voltage bidirectional current sense amplifiers from ADI, such as the model AD8210 or AD8211, which have gains of 20 and common mode voltages of up to 65V. To evaluate the shunt, Bourns tested its Model CSM2F-8518 (100µohm nominal resistance), as shown in Figure 2. A single-board microcontroller kit is programmed to communicate with the module over an SPI connection. The Figure 3 Data in Degrees Celsius Recorded by the Module Figure 4 Data in Millivolts Recorded by the Current Sense Module current for the measurement was generated using a precision current source. The first measurement to be determined is the resistance of the shunt. This is done using the known current from the current source and a precision 4-wire voltmeter. Once the actual resistance of the shunt is measured, then the voltage across the shunt using the current sense module can be compared with the actual resistance value. The current sense amplifier has a common mode voltage of 80V maximum, allowing for the module to be placed at the high end in 48V battery systems. The module also contains a surface mount temperature sensor with a PWM output proportional to the ambient temperature. Figure 3 shows the temperature sensor output at room temperature. The amplifier power is supplied by a DC supply of +5V. This experiment's power comes from a Low Drop Out (LDO) regulator with the original supply coming from the USB interface. For an isolated 5V supply, a low-power micro converter using the ADI LTC8301 (flyback or push-pull) can provide the necessary isolation with the required safety level. Figure 4 shows the data points collected from the A/D input terminals with an average of 22.44364mV and peak- to-peak variation of 0.007mV over the sampling period. Determining Measurement Accuracy The accuracy of the measurements at room temperature can be calculated using the following formula. The accuracy: (Expected Voltage-Actual Measurement)mV*100 Full Range of Op Amp Figure 2 Block Diagram of Signal Processing Circuit and Photo of Experiment

Articles in this issue

Links on this page

view archives of Supplier eBooks - Bourns - Achieving Enhanced Performance and Reliability