Supplier eBooks

Bourns - Achieving Enhanced Performance and Reliability

Issue link: https://resources.mouser.com/i/1442856

Contents of this Issue

Navigation

Page 26 of 27

Figure 6 Data from Lookup Table Showing Resistance Drift with Temperature | 27 | LEARN MORE MODEL CSM2F HIGH POWER CURRENT SENSE RESISTORS LEARN MORE CURRENT SENSE RESISTORS Figure 5. Accuracy of Bourns® Model CSM2F-8518 Shunt with Current Sense Module The data at several DC currents ranging from 10mA up to 20A was recorded, and the accuracy calculated (shown on the graph in Figure 5). The accuracy tends to degrade once the currents increase beyond 10 amperes, and the shunt starts to heat up. The resistance value used to calculate the current will drift as a result, which has a negative impact on the accuracy of the measurements. To further assist designers, Bourns has developed a look-up table that shows the normalized increase or decrease of the resistance with temperature. With this data, the original value used for the resistance can be modified by the factor shown in Figure 6 and correlated with the temperature sensor reading. Helping to Ensure BMS Safety and Long Life Currents of several hundred amperes are measured by BMS in various e-mobility applications during battery charging and discharging. The ability to measure current accurately provides critical information for safety and ensures long battery pack life. Using an ultra-low resistance shunt resistor and a precision AFE can provide very accurate readings from very high to very low current levels with accuracy tolerances of less than 0.01 percent. Also, temperature sensing, and lookup tables from Bourns, can improve measurement accuracy as the temperature increases. This application note has provided a proven methodology to measure the cell voltage, temperature, and current to determine the state of health of a battery cell. Key in this process are Bourns ® current sense amplifiers featuring low offsets and high common mode voltages that enable high accuracy with the shunt being placed at the high end in 48V applications. Bourns ® Model CSM2F Series shunt resistors are manufactured in an International Automotive Task Force approved facility certified to build components for certain harsh environment applications such as in high energy BMS used in HEVs and BEVs. ■

Articles in this issue

Links on this page

view archives of Supplier eBooks - Bourns - Achieving Enhanced Performance and Reliability