Supplier eBooks

Texas Instruments - The Future of Robotics

Issue link: https://resources.mouser.com/i/1442859

Contents of this Issue

Navigation

Page 10 of 35

Texas Instruments The Future of Robotics | 11 Figure 4: Texas Instruments PGA460/PGA460-Q1 Ultrasonic Processor & Driver is a highly integrated system-on-chip ultrasonic transducer driver, and a signal conditioner with an advanced DSP core. Figure 5: Texas Instruments TUSS4470 Direct Drive Ultrasonic Sensor IC is a highly integrated transformer drive analog front end for industrial ultrasonic applications. The components of an ultrasonic-based obstruction avoidance system used in autonomous robotic systems might include an ultrasonic signal processor and transducer driver, such as the Texas Instruments PGA460/PGA460-Q1 Ultrasonic Processor & Driver, a highly integrated system-on-chip ultrasonic transducer driver, and a signal conditioner with an advanced DSP core (Figure 4). It drives the transformer, processes the returned electrical signals from the echoes, and calculates the ToF data for each of the relevant echoes in real-time. The device has a complimentary low-side driver pair that can drive a transducer either in a transformer-based topology using a step-up transformer or in a direct-drive topology using external high-side FETs. The PGA460/PGA460-Q1 can receive and condition the reflected echo signal for reliable object detection. This feature gets accomplished using an analog front-end (AFE) consisting of a low-noise amplifier followed by a programmable time-varying gain stage feeding into an ADC. The digitized signal is then processed in the DSP core for both near-field and far-field object detection using time-varying thresholds. Other designs might benefit from Texas Instruments TUSS4470 Direct Drive Ultrasonic Sensor IC, a highly integrated transformer drive analog front end for industrial ultrasonic applications (Figure 5). The transducer drive stage is an internal H-bridge that can be configured to drive the transducer in direct-drive mode to achieve maximum voltage across the transducer. The internal H-bridge can also be configured as a pre-driver for external FETs, enabling higher current and voltage drive for larger transducers.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Texas Instruments - The Future of Robotics