Supplier eBooks

Kemet - 7 Experts on New Approaches for Power Distribution Network Design

Issue link: https://resources.mouser.com/i/1442868

Contents of this Issue

Navigation

Page 4 of 30

5 "Gallium nitride power transistors, which can replace silicon metal oxide semiconductor field-effect transistors, enable much higher-frequency switching with greater efficiencies." Benoit GORAL, Signal and Power Integrity Engineer, Thales Benoit Goral holds a PhD from Université Paris-Saclay. His research, in collaboration with Thales Communications and Security, focuses on power integrity and power rail design optimization. Since 2017, he has worked with Thales SIX GTS France, where he is in charge of high-speed, complex PCB design; high-speed serial link development; DDRx interface simulation and optimization; and equipment-level EMC design and troubleshooting. Many of our products are avionics and tactical communication related, so our designs must work reliably for many years in harsh environments and extreme temperature ranges. For that reason, we use proven parts rather than leading-edge technologies. Our critical constraints are size, weight, and power. Cost is not so important because we manufacture highly specialized devices with low production runs. One challenge we face is power distribution network (PDN) size. On a digital board, the PDN that distributes power to components can take as much as 30 percent of the surface of the printed circuit board (PCB). To make the device smaller, we must optimize the PDN, but conflicting trends make this difficult. For example, we can reduce the size of the PDN by using an integrated circuit (IC) that implements up to eight DC-to-DC converters in one IC package. The resulting component is not a digital component but an electronic power component that is a single package with one power input and up to eight different power rails on the output side. This approach, in combination with much smaller decoupling capacitors in a 0201-inch package size or smaller, helps reduce overall PDN size. System-on-a-Chip Components Create PDN Challenges 5

Articles in this issue

Links on this page

view archives of Supplier eBooks - Kemet - 7 Experts on New Approaches for Power Distribution Network Design