29
Pranav Devalla, Hardware Design
Engineer, Arista Networks
Pranav Devalla is a system hardware
design engineer at Arista Networks,
working on next-generation data center
switch systems. He focuses on system
signal and power integrity and has
extensive experience in validating complex
PCB designs using advanced simulation
and measurement techniques. In his
previous role, he was an electromagnetics
applications engineer at Ansys Inc. He
holds a master's degree in electrical and
computer engineering from Colorado
State University.
Power distribution networks (PDNs) are designed to accomplish two things. First, they
must deliver the required DC power without dropping voltage, and second, they must
have enough capacitance to supply current to whatever devices need the current.
Every application has constraints that affect PDN design. For example, consumer
electronics have more constraints in terms of using the lowest-power and least
expensive components, and they must meet a different set of regulations compared
with equipment used in data centers or industrial applications.
Simulation is an essential tool for balancing the many physical and design constraints
that must be resolved in a successful PDN solution. However, even simulation tools can
only get you so far because trends in device design requirements make achieving the
essential PDN objectives more difficult.
For instance, over the past ten years, we have seen semiconductor process size shrink
from 65 nanometers to 7 nanometers and now 5 nanometers. Chip manufacturers
are working on designs that use 3- and 2-nanometer nodes. These small process
sizes use fin field-effect transistors (FETs) and gate-all-around FETs that operate with
higher switching speeds and lower voltages, and that is resulting in scaling down the
voltage requirements of these devices. At the same time, with smaller process sizes,
chip manufacturers are able to pack more and more onto a single chip, which increases
Simulations Have Limitations
"As voltage drops and operating voltage ranges grow
narrower, devices become more susceptible to noise."