Supplier eBooks

Wurth - Behind the Mystery of Electromagnetic Compatibility Design

Issue link: https://resources.mouser.com/i/1447260

Contents of this Issue

Navigation

Page 16 of 25

Würth Elektronik 2022 17 Figure 7: EMC measurement with input filter and aluminum polymer capacitor C IN (Source: Würth Elektronik Group) -20 0 20 40 60 80 100 100 kHz 1 MHz 10 MHz dBµV Frequency Average QPeak CISPR 32 Average CISPR 32 QPeak 30 MHz 150 kHz It can be seen that by changing only one component, the EMC performance was significantly improved. The voltage drop generated by the fundamental frequency and the first harmonic of this frequency are reduced, generating less interference. However, the limit could not be met, so further filters have to be placed. The structure of the input filter was based on datasheet information. The filter's insertion loss (in a 5Ω system) is shown in Figure 6. The input filter was then included on the PCB, and another measurement was performed. The result is shown in Figure 7, where the interaction between the aluminum polymer capacitor and the input filter is visible. The combination of input filter and low ESR and low ESL of the polymer electrolytic capacitance make it possible to push the level broadband below the limit of class B. Values of less than 40dBμV (average and quasi peak) are easily possible (compared to the first measurement with around 100dBμV), so the measurement is passed. Figure 6: Built-in input filter with simulated filter performance (Source: Würth Elektronik Group) -140 dB -120 dB -100 dB -80 dB -60 dB -40 dB -20 dB 0 dB 100 kHz 1 MHz 10 MHz 100 MHz 1 GHz Frequency Attenuation

Articles in this issue

view archives of Supplier eBooks - Wurth - Behind the Mystery of Electromagnetic Compatibility Design