Supplier eBooks

Wurth - Behind the Mystery of Electromagnetic Compatibility Design

Issue link: https://resources.mouser.com/i/1447260

Contents of this Issue

Navigation

Page 15 of 25

Behind The Mystery of Electromagnetic Compatibility Design 16 Figure 5: EMC measurement with an aluminum polymer capacitor as input capacitor C IN (Source: Würth Elektronik Group) It can be seen that the limit values of CISPR 32 class B are exceeded. Noise levels of up to 100dBμV are detectable. But where do these interfering signals come from? The capacitor as a real component has parasitic effects, particularly the ESR and the parasitic effects of the layout (the lead inductance) generate a high-frequency voltage drop that can be detected by measurement. This is shown schematically in Figure 4. An aluminum polymer capacitor can be used as a first approach to achieve acceptable levels of emissions and stay below the limits. The aluminum polymer capacitor's electrical properties in terms of capacity and rated voltage are the same as those of the aluminum electrolytic capacitor. The design is also equivalent at the capacitance of 47μF, and the capacitor fits the original land pattern. The aluminum polymer capacitor used was a WCAP-PSLP 875 105 344 006 (Link to REDEXPERT) with a capacitance of 47μF, rated voltage of 16V, and an ESR of 20.7mΩ and ESL of 3.9nH. Because of the very low ESR and ESL, the following measurement of the interference spectrum is achieved (Figure 5). R EQ,C C IN L EQ,C U IN U SUPP L SUPP,1 L SUPP,2 R SUPP,2 R SUPP,1 f RES C IN i IN i IN - i C,IN -20 0 20 40 60 80 100 100 kHz 1 MHz 10 MHz dBµV Frequency Average QPeak CISPR 32 Average CISPR 32 QPeak 30 MHz 150 kHz Figure 4: Schematic representation of the cause of the disturbances (Source: Würth Elektronik Group)

Articles in this issue

Links on this page

view archives of Supplier eBooks - Wurth - Behind the Mystery of Electromagnetic Compatibility Design