Supplier eBooks

Wurth - Behind the Mystery of Electromagnetic Compatibility Design

Issue link: https://resources.mouser.com/i/1447260

Contents of this Issue

Navigation

Page 21 of 25

Behind The Mystery of Electromagnetic Compatibility Design 22 Otherwise, this might cause uncontrolled turn-on/off of the MOSFET and thermal issues. Some SiC MOSFETs are designed with an additional low-impedance Kelvin source connection (Figure 4) for a gate current return path. This connection does not carry the high switching current and has a lower interference potential than the source connection, which significantly improves gate driving (such as Infineon IMZ120R045M1 1200V/52A), Regarding the auxiliary supply, it should be compact with its output capacitors (with minimal ESL and ESR) placed very close to the gate driver and SiC/GaN device to minimize the gate current loop and associated parasitic effects. Isolated Gate Driver Power-Supply Requirement A large selection of compact, isolated 1 – 2W DC/DC converters are available on the market. For a SiC-MOSFET such as the Infineon IMZ120R045M1 1200V/52A, up to 1W power requirement per device can be estimated (see example calculation (1)). However, an application with over 5kW load power would require the use of either a SiC-MOSFET module (ROHM BSM600D12P3G001 1200V/600A) or alternatively several discrete SiC-MOSFETs in parallel (current sharing). In a module solution, several semiconductor dies are paralleled to form the final SiC-MOSFET. This technique reduces the effective R DS(ON) but results in a very high Total Gate Charge, which places a higher power requirement on the gate-driver system power supply (example calculation (2)). Above 2W of power, a limited number of off-the-shelf isolated DC-DC converter modules are available. Despite their convenience, the modules are often large, weighty, expensive, and with efficiencies lining under 79 percent. P Gate Total power required to drive the SiC device gate P Driver Power loss in the gate driver section (approx. 0.3W) Q Gate Total Gate Charge value (from datasheet) F SW Maximum switching frequency ∆V Gate Maximum voltage swing at the gate from –V ee to +V dd (e.g. -4V to +15V = 19V) Example calculation (1) with Infineon IMZ120R045M1 1200V / 52A: Example calculation (2) with ROHM BSM600D12P3G001 1200V / 600A: Figure 4: Kelvin connections and critical parasitic inductances in a half-bridge configuration. (Source: Würth Elektronik Group)

Articles in this issue

Links on this page

view archives of Supplier eBooks - Wurth - Behind the Mystery of Electromagnetic Compatibility Design