Supplier eBooks

Bourns - 8 Experts on Magnetic Solutions for Next-Generation Applications

Issue link: https://resources.mouser.com/i/1471851

Contents of this Issue

Navigation

Page 11 of 23

"Custom magnetics can help meet a system's specific needs in terms of frequency response, performance, size, and cost." Dr. Thomas Yilun Luo Advanced Power Inverter Design and Analysis Engineer, General Motors In the design of magnetics for signal transmission applications, the construction of the component again becomes the determining factor of its performance. For example, to ensure the transmissibility of their signals, engineers must use magnetics designed with appropriate core materials. Important considerations for core materials include their current capacity and behavior at a given frequency, such that the component meets the requirements of the system. The windings must then be appropriately balanced around the core, while considerations of size will further impact performance versus frequency. In signal transmission, the first two questions you need to ask are 'Is the application isolated?' and 'How faithfully reproduced does the data stream need to be?'. From there you can design magnetics that meet the signal transmission requirements. Kyle Moldenhauer Field and Applications Engineer, Bourns, Inc. 12 I Magnetic Components for Signal Transmission Bourns offers solutions for signal transmission that do the following: • Cover a wide variety of protocols and applications • Help balance trade-offs among cost, performance, and size of components to simplify the designer's job • Use the best core materials and winding geometries to ensure maximal performance and reliability for a given application

Articles in this issue

view archives of Supplier eBooks - Bourns - 8 Experts on Magnetic Solutions for Next-Generation Applications