Supplier eBooks

NXP - 7 Experts on Designing Vehicle Electrification Solutions

Issue link: https://resources.mouser.com/i/1496365

Contents of this Issue

Navigation

Page 16 of 22

C h a p t e r 4 DESIGNING FOR EFFICIENCY Achieving the best driving range possible is arguably the most significant challenge that EV designers face. On the lowest level, this means designing a vehicle that can most effectively store electrical energy and convert it into usable kinetic energy for driving. EV designers should strive to create the most efficient vehicle electrification systems possible. On a high level, electrical efficiency is important because it will play a significant role in determining how much stored electrical energy can be converted into usable driving energy. Beyond this, however, electrical efficiency is an important metric for overall sustainability, which is the ultimate goal of EVs. While many different variables and subsystems impact a vehicle's efficiency, the EV powertrain is one area of particular interest. The EV powertrain is designed to take stored DC energy from the battery, convert it to AC, and supply that AC to the motor where it is converted to the kinetic energy of the spinning wheels. The powertrain's traction inverter—which is responsible for converting DC from the battery to AC for the motor—is especially important from an efficiency perspective. A typical traction inverter system consists of a BMS that controls the battery and charges a DC link capacitor. This provides the power to the traction motor controller, which consists of a motor control unit, Vincent McNeil Director of Segment Line, NXP Semiconductors If you consider an EV end to end, you have efficiencies going from the battery where you're storing the energy, down to the traction inverter, and then eventually into the spinning of the car wheels. A designer's goal is to maximize the efficiency of each of these systems." 17 7 Experts on Designing Vehicle Electrification Solutions

Articles in this issue

Links on this page

view archives of Supplier eBooks - NXP - 7 Experts on Designing Vehicle Electrification Solutions