Supplier eBooks

NXP - 7 Experts on Designing Vehicle Electrification Solutions

Issue link: https://resources.mouser.com/i/1496365

Contents of this Issue

Navigation

Page 8 of 22

Franck GaltiƩ Functional Safety Director, NXP Semiconductors C h a p t e r 2 Safety is one of the most significant considerations when designing vehicle electrification solutions. In the context of EVs, safety may be defined in many ways; with a focus on hardware, safety is best viewed as designing systems that exhibit the smallest probability of failure. Hardware designers should strive to design vehicle electrification solutions that are robust and reliable regardless of operating conditions, device age, or other environmental factors. Hence, safety is best defined as reducing the probability of a failure beneath some acceptable level. The problem with this definition, of course, is that the acceptable level of safety cannot be subjective; rather, it must be defined stringently to include passengers across the market. Thus, designers must aim to adhere to a number of different safety standards, such as the International Organization for Standardization's (ISO's) popular standard ISO 26262. By adhering to these standards, designers can meet different Automotive Safety Integrity Levels (ASILs), ranging from ASIL A on the low end to ASIL D on the high end. Achieving safety in EV design may be particularly difficult owing to the combination of high voltages, high DESIGNING FOR SAFETY For maximum safety, we need to analyze all types of failures from all levels, including looking individually at the system, hardware, and software. The goal is to identify all of the potential failure modes and find a way to avoid fatal failures or mitigate the effect of those failures." 9 7 Experts on Designing Vehicle Electrification Solutions

Articles in this issue

Links on this page

view archives of Supplier eBooks - NXP - 7 Experts on Designing Vehicle Electrification Solutions