Supplier eBooks

Renesas - Bringing Intelligence to the Edge

Issue link: https://resources.mouser.com/i/1499313

Contents of this Issue

Navigation

Page 26 of 27

Renesas 2023 27 Sensorless Motor Demo With support provided for the Renesas Motor Control Kits, one way to evaluate the features available through Reality AI Tools is by using an existing demo, such as the Reality AI demo on mouser.com. The demo incorporates the Renesas RA6T2 Motor Control Kit and provides insight and instructions for creating a predictive sensorless ML model that detects unbalanced motor loads using current, voltage, and speed. The RA6T2 Motor Control Kit features an enhanced central processing unit (CPU) and hardware accelerator for home appliance and industrial automation application deployments. The kit comes complete with all the basics, including a CPU board, inverter board, communication board, and brushless DC motor. The project article outlines the necessary resources and required hardware, with applicable links as well as steps to train and deploy your ML model. If you are looking to jump right in with Reality AI without the hardware, pre- built data files are also available to help you get started. The steps in the demo take you through everything from uploading and curating your data to training and deployment. Of course, this only scratches the surface of the entire suite of available features, such as using new data to further test and optimize as well as ways to potentially decrease the complexity of the model without sacrificing accuracy. An example of a simple application for this type of demo is detecting issues with load balance in a washing machine during a spin cycle and notifying the end user. Conclusion Renesas Reality AI is a powerful software toolset that can revolutionize the way businesses analyze sensor data. Through automated analysis and selection of the most relevant sensor data for the specific prediction model Learn More RA6M4 Evaluation Kit of interest, the Reality AI toolset extracts meaningful insights and offers potential BOM optimization. These capabilities can also be incorporated via firmware updates into existing systems without additional BOM costs. The models generated are extremely resource efficient, consuming insignificant CPU load so the MCU is practically free to perform all the usual tasks while incorporating these features. With its complete integration into the Renesas toolchain and full support for the MCU portfolio and development boards, the Reality AI toolset provides the speed and accuracy required to deliver the precision businesses expect to make sense of vast amounts of data, helping to minimize costly equipment downtime. ■

Articles in this issue

Links on this page

view archives of Supplier eBooks - Renesas - Bringing Intelligence to the Edge