Supplier eBooks

Analog Devices - Leading the Way to the Digital Factory

Issue link: https://resources.mouser.com/i/1499776

Contents of this Issue

Navigation

Page 9 of 25

Michal Brychta Principal Applications Engineer, Analog Devices C h a p t e r 2 A fundamental characteristic of the digital factory is the interconnectivity of devices on the factory floor. Between edge devices, sensors, and other miscellaneous field instruments, all devices vital to the factory's operation are expected to be interconnected to share data and operational status. Historically in process plants, often an extension of the factory enterprise, the prominent communication protocol has been a 4–20 mA current loop. First introduced in the 1950s, 4–20 mA works by communicating a sensor output via current signals ranging from 4 mA to 20 mA. While this protocol became an industry standard for several reasons, a major reason was its ability to support communication over long, kilometer-range distances, which are needed for process plants. Unfortunately, the 4–20 mA protocol has become mostly antiquated and is no longer a feasible solution on a modern, high-speed factory floor. The 4–20 mA communication protocol fails in that it has inherently slow speed and only offers one-directional communication. SEAMLESS CONNECTED FIELD INSTRUMENTS WITH ETHERNET-APL With Ethernet-APL, you have much more bandwidth so you can transmit more data and power to the edge. With these benefits, the edge in a digital factory is now capable of even more things—including sensor fusion, and even more sophisticated human- machine interfaces—than would've been possible with 4–20 mA." 10 Leading the Way to the Digital Factory

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - Leading the Way to the Digital Factory