Supplier eBooks

Analog Devices - Engineering a More Sustainable Future

Issue link: https://resources.mouser.com/i/1512203

Contents of this Issue

Navigation

Page 12 of 67

13 Engineering a More Sustainable Future | ADI VISIT ANALOG.COM X Printing X Extrusion X Machining X Robotics X Pick and place X Handling, and many others Thought Leadership Article Driving Higher Levels of Flexibility, Productivity, and Sustainability in Smart Manufacturing Maurice O'Brien , Strategic Marketing Manager The Importance of Intelligent Motion Control in Smart Manufacturing Intelligent motion control is the core building block of smart manufacturing, enabling highly flexible and efficient manufacturing. Intelligent motion control combines precision feedback, advanced sensing, high performance control, and seamless connectivity to deliver deterministic motion solutions. Seamless connectivity of motion insights to PLCs and manufacturing execution systems ( MES ) allows advanced analytics to optimize manufacturing flows and identify potential issues before production stops. Smart manufacturing using intel- ligent motion control can be reconfigured quickly to support more agile and scalable manufacturing, including batch size 1 production. By reducing the time to complete a manufacturing step and optimizing the manufacturing flow for higher throughput, less energy is consumed resulting in more sustainable smart manufacturing. Intelligent motion applications include: X Pumps X Fans X Hoists X HVAC X Conveyors X Winding The Evolution of Intelligent Motion Control Solutions Motion control has evolved over time, from simple grid connected motors to complex multi-axis servo drive solutions for machine tools and industrial robots. This evolution has been accelerated by the increasing complexity of automa- tion required to deliver higher levels of productivity, flexibility, and autonomy in smart manufacturing ( see Figure 1 ) . Grid-Connected Motor The most basic motion solutions are based on a grid-connected or AC-powered, 3-phase fixed speed motor that uses a switchgear to provide on/off control and protection circuitry. These basic motion solutions run at a relatively fixed speed, independent of any load variation. A reduction in output is implemented with mechanical controls—throttles, dampers, gears or valves, pumps, and fans are some typical asset examples. Inverter Driven Motor The addition of a rectifier, DC bus, and a 3-phase inverter stage in effect creates a variable frequency and variable voltage source that is now applied to the motor to enable variable speed control. This inverter driven motor enables significant reduction in energy consumption by running the motor at the optimum speed for the load and application. Examples include higher efficiency pumps and fans. Variable Speed Drive For higher performance motion control applications, a variable speed drive ( VSD ) enables accurate torque, velocity, and position control. To achieve this, current and position measurement are added into the basic open-loop inverter drive. More precise control of motor velocity, position, and torque is then possible. Conveyors, winding, printing, and extrusion machinery are typical examples of these applications. Servo-Driven System Synchronized, multi-axis servo-driven systems are used in more complex motion applications. Machine tools and CNC machines require synchronization of multiple axes, with extremely accurate position feedback. In CNC machining, 5-axis coordination is common, although there are applications that utilize up to 12 axes in which tools and workpieces are both being moved with respect to each other in space.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - Engineering a More Sustainable Future