Supplier eBooks

Analog Devices - Engineering a More Sustainable Future

Issue link: https://resources.mouser.com/i/1512203

Contents of this Issue

Navigation

Page 51 of 67

52 ADI | Engineering a More Sustainable Future Powering a 10BASE-T1L Sensor Prototype Figure 5 shows a power supply design for a digital wired MEMS sensor. The LT8618 is specifically designed for industrial sensors with: X Wide input range up to 60 V X Low output current 100 mA X Up to 90% efficiency X Tiny 2 mm × 2 mm LQFN packages Figure 5 shows the LT8618 with a 24 V DC input, which is regulated to 3.7 V, and then input to the LT3042, which supplies 3.3 V to the MEMS sensor circuitry. The LT3042 is a high performance ultralow noise LDO regulator with: X Ultralow rms noise at 0.8 µV rms (10 Hz to 100 kHz) X Ultrahigh PSRR (79 dB at 1 MHz) X Tiny 3 mm × 3 mm DFN packages The article "How to Get the Best Results Using LTspice for EMC Simulation—Part 1" 2 details an LTspice simulation circuit and discusses the EMC performance for the LT8618 and LT3042. Figures 19 and 20 from the article show simulation results for where an EMC disturbance is applied at the LT3042 input. This shows that the LT3042 has less than 200 µV of voltage ripple even in the presence of a 1 V p-p EMC disturbance at its input. Integrating a Digital Hardware Design and a Mechanical Enclosure A steel or aluminum enclosure is used to house a MEMS vibration sensor and provide solid attachment to monitored assets, as well as providing water and dust proof-ness ( IP67 ) . For vibration sensors, the natural frequencies of the enclosure must be greater than that of the applied vibration load measured by the MEMS sensor. The frequency response plot for the ADXL1002 MEMS is shown in Figure 6. The ADXL1002 3 dB bandwidth is 11 kHz and it has a 21 kHz resonant frequency. A protective enclosure used to house the ADXL1002 needs to have a first natural frequency of 21 kHz or greater in the axis of sensitivity. Similarly, when designing a triaxial sensor, the natural frequencies of the mechanical enclosure need to be analyzed across vertical and radial directions. Sensor prototypes are tested on modal shakers, which provide a controlled environment to set vibration test levels and sweep across frequency. The test results of sensor frequency response should closely follow the MEMS sensor information shown in Figure 6. Modal Analysis Modal analysis is a commonly used technique to provide a good understanding of the vibration characteristics of enclosures. Modal analysis provides the natural frequencies and normal modes Adobe Stock / Mentor56 – stock.adobe.com

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - Engineering a More Sustainable Future