Supplier eBooks

Murata - 9 Industry Experts Discuss MEMS Technology

Issue link: https://resources.mouser.com/i/1516604

Contents of this Issue

Navigation

Page 4 of 27

C h a p t e r 1 One application that most powerfully demonstrates the value of MEMS is the IMU. An IMU is an electronic device that measures and reports a body's specific force, angular rate, and sometimes magnetic fields. These measurements are collected by leveraging and aggregating data from a combination of accelerometers, gyroscopes, and magnetometers. Thanks to the integration of multiple sensors into one unit, IMUs provide a valuable tool for determining the relative positioning and orientation of a device. Alongside the possible introduction of GPS, IMUs have proven to be particularly important in applications that require navigation or autonomy, such as vehicles and industrial equipment. Consider the example of a construction machine. In an excavator, IMUs allow the machine to understand its positioning to control digging depth with a high level of accuracy and automation. As the excavator operates, the IMU continuously measures and reports on parameters like tilt, roll, and pitch. These measurements are crucial for ensuring that the digging arm moves exactly as intended, avoiding over or under digging. Before the introduction of MEMS, IMUs were based on very cumbersome equipment that included some combination of fiber optics, lasers, and/ MEMS AND IMUS Abhilash Joshi Senior Design Engineer, Sweco The technologies used for accurate slope or position measurements have evolved significantly over the years. For instance, inertial navigation systems (INS) use accelerometers and gyroscopes to measure changes in velocity and orientation where GPS may not be available or reliable." 5 9 Industry Experts Discuss MEMS Technology

Articles in this issue

Links on this page

view archives of Supplier eBooks - Murata - 9 Industry Experts Discuss MEMS Technology