Supplier eBooks

STMicroelectronics - Beyond the Wires: Exploring Bluetooth and LoRaWAN Connectivity

Issue link: https://resources.mouser.com/i/1520713

Contents of this Issue

Navigation

Page 12 of 27

STMicroelectronics 2024 13 STM32WBA5 Multiprotocol Wireless Radio MCU Learn More STM32WBA55G-DK1 Discovery Kit Learn More BIS can be used to broadcast gate announcements at an airport terminal, or music to attendees at a concert, among many other use cases. BIS is the mode underlying the audio broadcasting capabilities that the Bluetooth organization has branded as Auracast™ (Figure 2). Inherent with BIS/CIS is the ability of both sources and sinks to handle multiple channels simultaneously. This ensures that an earbud user could be listening to music from their smartphone and monitoring public-address announcements at the same time. Now, let's take a closer look at broadcast mode. Under Bluetooth Classic, connections are 1:1—one source connected to one sink. Bluetooth LE Audio allows a source to simply broadcast streams of packets to whoever might be listening. This ability of a source to simply broadcast content, allowing users to subscribe if they wish, opens new categories of use cases, from individuals sharing content Broadcast Sink Broadcast Sink Broadcast Sink Broadcast Source Train Station Announcements Audio Streams Broadcast Use Case Figure 2: Example of a broadcast use case. (Source: Mouser Electronics) with each other to delivering messages or music in crowded public spaces. Bluetooth SIG has branded a collection of these capabilities as Auracast. But broadcast raises an issue with the way to handle data integrity. Bluetooth Classic assumes every data transaction must be lossless. If a packet is dropped or corrupted, the source device will repeat the transmission until it receives a positive acknowledgment. Broadcast is inherently unidirectional, so acknowledgments are not possible. Rather than waiting for an acknowledgment, broadcast mode will continue on, depending on LC3's packet loss concealment (PLC) algorithm in the receiving device to reconstruct the missing data so that the loss is inaudible. It is also possible for broadcast mode to do multiple retransmissions to ensure that a wide variety of receiving devices in different reception environments get a usable copy of the data.

Articles in this issue

Links on this page

view archives of Supplier eBooks - STMicroelectronics - Beyond the Wires: Exploring Bluetooth and LoRaWAN Connectivity