Supplier eBooks

STMicroelectronics - Beyond the Wires: Exploring Bluetooth and LoRaWAN Connectivity

Issue link: https://resources.mouser.com/i/1520713

Contents of this Issue

Navigation

Page 7 of 27

Wireless modules are usually straightforward to integrate into a design and pair with a compatible main MCU to offer a complete IoT solution. With a wireless module, the design team doesn't need to worry about developing a certification- and regulation-passing wireless communications circuit, which can dramatically reduce costs and development time. Additionally, product line diversity can be achieved by using different wireless modules—or even the same wireless module with different programming—to operate with various wireless standards. Wireless Modules vs. Wireless MCUs for 2.4GHz and Sub-GHz IoT Applications With both 2.4GHz and sub-GHz frequency ranges well- suited for most IoT applications, there are many approaches and product options for designing IoT solutions in these ranges. Some groups choose to go with a wireless MCU SoC and design their wireless communication circuit instead of selecting a prebuilt wireless module. However, to make " With a wireless module, the design team doesn't need to worry about developing a certification- and regulation-passing wireless communications circuit. a wireless MCU solution viable, a design group needs RF design/engineering expertise, lab equipment, RF sourcing expertise, RF PCB design skills, and antenna design and fabrication capability, and the entire solution would then need to be separately certified. On the other hand, a wireless module is a drop-in solution that can alleviate the need for additional development work aside from software development for programming the module. Conclusion For a given application, there are a variety of factors to keep in mind when selecting between wireless MCUs and wireless modules. Wireless modules have higher per-chip costs than wireless MCU SoCs. Depending on the production volume of an IoT product, designers may incorporate a wireless MCU with a low per-unit cost where the RF design and development costs would be divided among a large number of parts. This could result in a lower cost of production than a wireless module, which may also not be available at specific volumes desired, depending on the supply chain for the part. Beyond the Wires 8 STM32WB1MMC BLUETOOTH ® Low Energy Module Learn More Discovery Kit with STM32WB5MMG MCU Learn More

Articles in this issue

Links on this page

view archives of Supplier eBooks - STMicroelectronics - Beyond the Wires: Exploring Bluetooth and LoRaWAN Connectivity