Supplier eBooks

STMicroelectronics - Beyond the Wires: Exploring Bluetooth and LoRaWAN Connectivity

Issue link: https://resources.mouser.com/i/1520713

Contents of this Issue

Navigation

Page 18 of 27

STMicroelectronics 2024 19 allows for internal security, rapid response times to events, and the eventual backhaul to an internet connection through a secured hub. In addition, the network can easily be expanded to accommodate many nodes that may be in a physically close area. The key contribution of this topology is that it is private and controls a specific function. To address these use cases, the STM32WL is used as the basis of a new network architecture that delivers an expanded-footprint, mobility-capable private network using GFSK modulation. The keys to delivering this successfully are the implementation of a hub-node architecture (Figure 2) and the ability of the hubs and nodes to operate in peer- to-peer mode. Compared with a typical LoRaWAN network, the distribution of nodes is tightly controlled over a much shorter distribution distance profile, allowing hubs and nodes to interact with each other. In this architecture, general nodes (as opposed to relay nodes, which will be discussed later) are associated with one hub, thus creating a network of devices. A general node is typically a device that hosts sensors and/or GPS Master 1 Node 2 Node 1 Master 1 Node 2 Node 1 Relay Figure 2: Typical multi-node and network extension model. (Source: STMicroelectronics)

Articles in this issue

view archives of Supplier eBooks - STMicroelectronics - Beyond the Wires: Exploring Bluetooth and LoRaWAN Connectivity