Supplier eBooks

STMicroelectronics - Beyond the Wires: Exploring Bluetooth and LoRaWAN Connectivity

Issue link: https://resources.mouser.com/i/1520713

Contents of this Issue

Navigation

Page 4 of 27

STMicroelectronics 2024 5 Creating Compliant Devices To meet market expectations and to comply with tougher incoming legislation, device manufacturers need to ensure that the platforms and ecosystems powering their development can enable them to certify their products successfully. ST's latest STM32 wireless microcontrollers (MCUs) are at the heart of next-generation devices that must satisfy legislation such as EU RED and U.S. Cyber Trust Mark. In fact, this product is already certifiable according to SESIP Level 3. Designers using ST wireless MCUs, such as the STM32WBA5 series, can take advantage of hardware features built into the silicon when creating wireless IoT devices. Security starts with the Arm ® Cortex ® -M33 core— designed with Arm's TrustZone ® architecture that allows an isolated secure area—running on a secure operating system and preventing access by non-secure software. TrustZone ensures security begins from the lowest level, the physical layer, which includes securing the boot and firmware update processes. STM32WBA5 Multiprotocol Wireless Radio MCU Learn More Moreover, the MCUs are compliant with the Arm Trusted Base System Architecture (TBSA), which requires hardware features including a root of trust (RoT), protected keystore, random number generator to support cryptography, and hardware cryptographic acceleration. These components ensure the correct security properties and can be maintained without compromising real-time application performance. The STM32WBA5 MCUs include a secure AES coprocessor and public key accelerator (PKA), both incorporating resistance to differential power analysis (DPA), and a HASH hardware accelerator. The MCUs also support secure firmware updates for over-the-air or local updating of

Articles in this issue

Links on this page

view archives of Supplier eBooks - STMicroelectronics - Beyond the Wires: Exploring Bluetooth and LoRaWAN Connectivity