Supplier eBooks

onsemi - Enabling a Sustainable Future with Silicon Carbide Power Electronics

Issue link: https://resources.mouser.com/i/1522571

Contents of this Issue

Navigation

Page 6 of 24

The fundamental advantages of SiC over Si are higher breakdown voltage and high thermal conductivity. Higher breakdown voltage allows a thinner drift layer and lower on-state resistance. This means conduction losses are less, and overall efficiency and power density are improved." C h a p t e r 1 | U n d e r s t a n d i n g t h e S i C R e v o l u t i o n more efficient power systems than those of silicon- based systems. Such design is extremely important in applications like EVs, for which decreased system weight directly translates into increased driving range. Additionally, more efficient power systems enable faster vehicle charging, greater utilization of stored energy, and extended driving ranges. Beyond the exceptional material properties of SiC, recent manufacturing and device packaging advances are also catalyzing its adoption. Modern advances in SiC wafer fabrication have created wafers with lower defect content, making SiC more affordable and reliable for end users. Additionally, new packaging is enabling SiC to gain widespread adoption. SiC boasts superior thermal conductivity (about 3 to 4.9 W/cm·K) compared to silicon (about 1.5 W/cm·K), necessitating packaging materials and techniques that can do the same. Recent innovations such as top-side and double- sided cooling packages enable SiC devices that can support greater temperatures and current densities than previously. Jayaram Subramanian High Voltage Systems Engineer, Mercedes-Benz Research & Development North America, Inc. 7 Enabling a Sustainable Future with Silicon Carbide Power Electronics

Articles in this issue

Links on this page

view archives of Supplier eBooks - onsemi - Enabling a Sustainable Future with Silicon Carbide Power Electronics