Supplier eBooks

Cinch - Understanding Harsh Environments for Electronic Design

Issue link: https://resources.mouser.com/i/1527887

Contents of this Issue

Navigation

Page 7 of 27

C h a p t e r 1 | W a t e r a n d E l e c t r i c i t y A specific consideration in the interconnection market is that connectors are usually used in mating pairs. A sealed or IP-rated connector is frequently sealed against harsh environments only when mated. If left unmated—for example, during installation or maintenance—the connector may not be protected. Connectors designed for service in harsh environments must be sealed against water, dirt, and dust; providing this protection requires careful consideration of design features. The most important area of sealing is between the face of the male and female connector, which is achieved through the use of a doughnut-shaped O-ring. Locking the mating halves of the connector in place provides the force required to compress the O-ring between the male and female connectors, creating a watertight seal. Preventing water ingress around the cable entry is also necessary. Because most cables are circular in cross-section, a simple rubber gland or gasket can be used. Robustness encompasses not only the durability of a connector and its ability to endure multiple cycles but also its adaptability to specific applications. Designers must consider the available options and select connectors appropriate for the application requirements and the expected service life." Carlos González Avelino Product Development Test Engineer, Philips Micro Devices 8 Understanding Harsh Environments for Electronic Design

Articles in this issue

Links on this page

view archives of Supplier eBooks - Cinch - Understanding Harsh Environments for Electronic Design