Supplier eBooks

Cinch - Understanding Harsh Environments for Electronic Design

Issue link: https://resources.mouser.com/i/1527887

Contents of this Issue

Navigation

Page 14 of 27

C h a p t e r 3 Hazards include those that are not visible but have a measurable impact on the reliability of any device. Unlike the expected presence of chemicals or moisture in some applications, these hazards cannot be truly quantified until a piece of equipment is in use. Therefore, they demand that the designer plans carefully to fully mitigate their dangers. Shock and Vibration Many devices must withstand constant shock and vibration during their operational lifespan. While this requirement may be expected in automotive and aerospace applications, vibration is also common in industrial machinery devices. Shock and vibration are hazards with both immediate and long-term effects. Short-term consequences include accidental disconnection of equipment. Long-term damage is harder to identify. Vibration causes individual components to rub together, causing significant damage over time, including wearing down of protective or conductive coatings and physical damage to components such as electrical contacts. In turn, issues ranging UNSEEN HAZARDS – SHOCK, VIBRATION, AND ELECTROMAGNETISM Rahul SreeKumar Senior Engineer, Nordex Group One of the conditions we design for is extreme temperatures, which can lead to thermal stress, vibration, and shock. These factors can loosen connections and result in fatigue failure of critical components." 15 Understanding Harsh Environments for Electronic Design

Articles in this issue

Links on this page

view archives of Supplier eBooks - Cinch - Understanding Harsh Environments for Electronic Design