Supplier eBooks

NXP - 11 Experts Discuss Advanced Motor Control for Modern Electric Vehicles

Issue link: https://resources.mouser.com/i/1529099

Contents of this Issue

Navigation

Page 6 of 25

A model-based design approach can help engineers identify performance changes and classify the severity of issues. Designers can then adjust the control structure to prevent failure, underperformance, or inefficiencies in the motor's operation." C h a p t e r 1 | A d v a n c e d A c t u a t i o n S y s t e m s i n t h e Ve h i c l e C h a s s i s performance. For instance, if a sudden load change occurs, the MCU can rapidly adjust the voltage applied to the motor phases to compensate, ensuring stable and efficient operation. Implementing such control systems in smart actuators presents several design challenges for engineers. For example, a tradeoff exists between low power consumption and precision control. High- precision control requires increased sampling and switching frequencies, which, in turn, demand more power. This behavior creates a balancing act where engineers must optimize the system to achieve the necessary precision without excessively increasing power consumption. Additionally, the real-world limitations of switching devices, such as metal-oxide-semiconductor field- effect transistors (MOSFETs), further complicate this balance. These components are designed for specific frequency ranges; pushing them beyond these limits can lead to inefficiencies and potential failures. For these reasons, the industry is starting to adopt new materials like gallium nitride (GaN) and silicon carbide (SiC), which can offer higher Marius-Lucian Andrei Technical Lead, Model-Based Design Team, NXP Semiconductors 7 11 Experts Discuss Advanced Motor Control for Modern Electric Vehicles

Articles in this issue

Links on this page

view archives of Supplier eBooks - NXP - 11 Experts Discuss Advanced Motor Control for Modern Electric Vehicles