Supplier eBooks

Analog Devices - 14 Experts Discuss Motor Control in Modern Applications

Issue link: https://resources.mouser.com/i/1530688

Contents of this Issue

Navigation

Page 14 of 26

Sustainable growth is a key challenge. At ADI Trinamic, we design efficient IC products that minimize energy use, enhance customer experience, and reduce reliance on external resources through intelligent control interfaces and advanced algorithms." C h a p t e r 2 | E n e r g y E f f i c i e n c y a n d M o t o r D r i v e S y s t e m s And this is a true challenge with today's pace of innovation and product development. This is why highly integrated solutions are the driver for a highly flexible and innovative industry. Motor drives can also significantly contribute to how efficiently systems operated by motors consume energy. As mentioned previously, historically, many motor-driven loads have been operated at fixed speeds because of the motor's direct grid connection. Regulation of load operation must then be carried out by mechanical means such as mechanical linkages or valves, and flow regulators in the case of fluidic systems. This regulation can have significant efficiency implications for systems operating at partial load or light load for substantial periods, as large gearing ratios or pressure drops must be sustained to match the motor's fixed speed with the load operating point. By contrast, inverter-fed motors allow precise control over motor speed and torque, enabling these parameters to be matched to the load operating point at all times. This matching can result in overall system efficiency improvements in Bernhard Dwersteg Principal Engineer, Analog Devices 15 14 Experts Discuss Motor Control in Modern Applications

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - 14 Experts Discuss Motor Control in Modern Applications