Supplier eBooks

Analog Devices - 14 Experts Discuss Motor Control in Modern Applications

Issue link: https://resources.mouser.com/i/1530688

Contents of this Issue

Navigation

Page 5 of 26

C h a p t e r 1 The landscape of motor control is diverse, with various motor types serving different industries and applications. Broadly, the major motor types are AC, brushed DC, stepper, and brushless DC (BLDC), each of which presents unique challenges and opportunities that engineers must address to optimize performance, reliability, and efficiency. AC Motors AC motors, particularly induction motors, are used in industrial applications because of their robustness and high-power capabilities. Historically, AC motors were operated directly from the grid, meaning that the motors operated at fixed speeds (with a very small variation of <5% over load). But, today's motors are increasingly driven by power electronics converters that sit between the AC grid and the motor. These power electronics converters consist of a rectifier that converts the AC input to a DC voltage, usually in the range of 400–1000V, and an inverter that converts the DC voltage to a variable-frequency, variable-voltage three-phase AC signal that drives the motor. MOTOR TYPES AND THEIR CONTROL CHALLENGES Thomas Ernst Staff Engineer, Product Applications, Analog Devices Understanding the capabilities and limitations of each motor type not only helps to lay out the motor control system properly. It can also enable the motor itself as a sensor, by using the feedback voltage of the motor optimally for advanced diagnostics and control algorithms to increase reliability and efficiency." 6 14 Experts Discuss Motor Control in Modern Applications

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - 14 Experts Discuss Motor Control in Modern Applications