Supplier eBooks

Analog Devices - 14 Experts Discuss Motor Control in Modern Applications

Issue link: https://resources.mouser.com/i/1530688

Contents of this Issue

Navigation

Page 9 of 26

sensorless control is often used in cost-critical systems where medium to ultra-high velocity motor control is needed, e.g., in blower applications. Typically, sensorless BLDC control does not allow for positioning and is therefore used for speed control up to very high velocities. Ensuring smooth, reliable, precise, and responsive control requires significant expertise and advanced algorithms that can be implemented in a dedicated chip set or a (32-bit) microcontroller. Stepper Motors Stepper motors are known for their ability to provide precise control, particularly at low speeds. These motors are widely used in applications requiring accurate positioning, such as semiconductor-handling robots, 3D printers, and surveillance cameras. Unlike traditional brushed DC or AC motors, stepper motors can operate in an open-loop system, meaning they do not require position or velocity feedback to maintain control. Further, their high torque, their ability to maintain position, and their high position resolution often enable them to work without any gearing. This architecture makes them cost-effective and easier to integrate into certain systems. However, the challenge with stepper motors lies in their torque curve. While stepper motors deliver high torque at low speeds, their torque rapidly diminishes as speed increases due to the feedback voltage (EMF). This feature limits their effectiveness in applications requiring both high C h a p t e r 1 | M o t o r T y p e s a n d T h e i r C o n t r o l C h a l l e n g e s Daniel Zaleski Product Applications Manager, Analog Devices For phase or inline motor control shunt-based current sensing, you have to be very robust against the PWM (pulse width modulation) stepping of the motor. The amplifier has to be very robust to reject the common-mode step and just amplify the differential voltage, which is representative of the current." 10 14 Experts Discuss Motor Control in Modern Applications

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - 14 Experts Discuss Motor Control in Modern Applications