Supplier eBooks

Analog Devices - Power Management: Efficiently Powering Processors, FPGAs, and Microcontrollers

Issue link: https://resources.mouser.com/i/1535932

Contents of this Issue

Navigation

Page 6 of 28

C h a p t e r 1 | W h a t I s P o w e r M a n a g e m e n t ? such as solar, into electrical energy for low-power applications using IoT devices at the edge, must also be managed. Thermal management also falls under the umbrella of power management— heat must be dissipated effectively and efficiently to ensure the device can be operated reliably and safely. Power management varies widely across devices Within the three broad categories of microcontrollers, processors, and FPGAs, a wide range of power management requirements exists. Microcontrollers fall at the lower end in terms of power— the loads are smaller, and their role is to control another device—and they are typically looking at different values and sensing different signals so they can send data over different interfaces. Microcontrollers have not only specific core voltages but also specific input/ output (I/O) voltage requirements. Processors also have stringent core voltage and I/O voltage requirements, especially higher-performance processors, which makes reliable power management more challenging. High-performance processors—both central processing units (CPUs) and graphics processing units (GPUs)—are found in data centers to support high-performance computing (HPC) and AI workloads, which consume significant power. GPUs, which are often used for deep learning, are especially power-intensive. FPGAs run the gamut in terms of power management. High-end FPGAs require many different voltage rails and significant power to support ultrafast computing of digital signals. Low-power FPGAs require only one or two voltages rather than the eight or more different voltages of higher-end FPGAs. A device at the far edge, whether a microcontroller, processor, or FPGA, may When choosing power or battery options, consider energy availability, peak and standby power consumption, and longevity requirements. Cost, form factor, and environmental conditions are also critical, especially in sensor nodes, where solar cells are often a primary choice." Luigi Fassio Senior Analog Design Engineer, Qualcomm 7 Power Management: Efficiently Powering Processors, FPGAs, and Microcontrollers

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - Power Management: Efficiently Powering Processors, FPGAs, and Microcontrollers