Supplier eBooks

Analog Devices - Power Management: Efficiently Powering Processors, FPGAs, and Microcontrollers

Issue link: https://resources.mouser.com/i/1535932

Contents of this Issue

Navigation

Page 10 of 28

C h a p t e r 2 Microcontrollers are everywhere today, embedded into a whole host of smart devices used in medical, agricultural, industrial, automotive, and instrumentation applications where they perform specific tasks. Often called an embedded controller or microcontroller unit, a microcontroller is essentially a small computer designed to control a small set of features within a larger device. Microcontrollers typically contain a central processor, memory, and I/O peripherals on a single chip. The processor interprets data collected via I/O peripherals, stores them in memory, and then communicates and acts in line with its purpose. From a power management perspective, a microcontroller is simpler than a CPU, GPU, or FPGA because its function is simply to look at different values and sense different signals, process them, and communicate them accordingly. Simpler microcontrollers have unique power management challenges Because microcontrollers' uses vary widely, their power management requirements differ—in some cases, they can be powered through energy harvesting or only require a small coin-sized battery with onboard power management. In the case of a microcontroller at the edge, looking at both the load and the source is critical— MICROCONTROLLERS AND POWER MANAGEMENT Power selection decisions for microcontroller-based systems should prioritize factors like power consumption, thermal and energy efficiency, and regulatory compliance within the application's constraints. For battery-powered designs, considerations must include capacity, rechargeability, and lifecycle cost." Jusuf Pratama Hardware Engineer, LG Electronics 11 Power Management: Efficiently Powering Processors, FPGAs, and Microcontrollers

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - Power Management: Efficiently Powering Processors, FPGAs, and Microcontrollers