Supplier eBooks

Microchip & Samtec - 8 Experts on PCIe for Emerging Embedded Systems

Issue link: https://resources.mouser.com/i/1542831

Contents of this Issue

Navigation

Page 16 of 28

Having a central PCIe bus allows a very high-throughput interface that could connect two systems. You still may have separate buses downstream in the system, but their size can be trimmed into something much more manageable and lower risk." C h a p t e r 2 | I n t e r c o n n e c t D e s i g n a n d S i g n a l I n t e g r i t y i n P r a c t i c e Once engineers route the design, post-layout simulation helps verify actual routing decisions. Engineers can use techniques such as eye-diagram and bathtub-curve analysis to identify hot spots or marginal channels that could fail at speed, allowing them to address issues long before fabrication. Beyond software, designers should validate assumptions on the benchtop. System-level evaluation kits offer a way to characterize full signal paths using real connectors and materials. This step is especially important for reducing risk in custom designs that deviate from standard PCI-SIG reference channels. Finally, OEMs should collaborate closely with interconnect manufacturers, silicon vendors, and system integrators to ensure the physical layer behaves predictably. Leveraging a manufacturer's shared reference designs can help design teams avoid common bottlenecks in grounding, via design, and breakout patterns. Jesse Hawkins Hardware Design Engineer, Tektronix 17 8 Experts Discuss PCIe for Emerging Embedded Systems

Articles in this issue

view archives of Supplier eBooks - Microchip & Samtec - 8 Experts on PCIe for Emerging Embedded Systems