Supplier eBooks

Vishay - An Automotive Grade Above

Issue link: https://resources.mouser.com/i/1429079

Contents of this Issue

Navigation

Page 11 of 27

12 \ VISHAY An Automotive Grade Above Figure 4: Simplified schematic of the main DC/DC converter stage (Source: Vishay) In the main DC/DC section of the charger (Figure 3 and Figure 4), the Vishay SQW61N65EF MOSFETs (M1-M4 and M5-M8 in Figure 4) are configured in H-bridges across the positive DC link stage (M1-M4) and the negative DC link stage (M5-M8 in Figure 4). The two stages are symmetrical, and each form an LLC resonant converter that switches from 150kHz to 250kHz. Each stage utilizes two transformers to minimize the size and profile compared to a single transformer implementation. The two stages work independently, but in the case of a difference in the respective output voltages, they shut down simultaneously to Figure 3: The 22kW OBC main DC/DC converter stage (Source: Vishay) " As the trend toward fast-charging systems continues, the power demanded from OBC has been steadily increasing from 5.5kW to 11kW, and now up to 22kW."

Articles in this issue

view archives of Supplier eBooks - Vishay - An Automotive Grade Above