Supplier eBooks

Vishay - An Automotive Grade Above

Issue link: https://resources.mouser.com/i/1429079

Contents of this Issue

Navigation

Page 18 of 27

mouser.com/vishay / 19 Learn More Learn More SQJQ144AE TrenchFET ® Gen IV Power MOSFETs VOMA617A Phototransistor Output Optocoupler (TR5/TR6 in Figure 2) and then filtered with a Vishay IHDM 2.5µH inductor (L2 in Figure 2) and C2 (in Figure 2) to provide 12V DC . The Vishay IHDM series is a customizable design in terms of inductance value, voltage rating, terminations, and mounting orientation. In order to minimize the MOSFET losses and keep the converter efficiency as high as possible, three SQJQ144AE devices were connected in parallel for each switch. The control signals for the low-voltage rectification MOSFETs are generated by the same control IC on the high-voltage side and transmitted to the low-voltage side using a pulse transformer to ensure that galvanic isolation is maintained. The voltage is measured on the output side and transmitted to the control IC on the high-voltage side using the Vishay VOMA617A optocoupler (Figure 3). An important parameter of this component is a high CTR (Current Transfer Ratio) with a low input current, and a high isolation test voltage (3750V RMS ) to maintain the galvanic isolation safely. A cost effective control method has been presented that provides the necessary galvanic isolation barrier between the high-voltage and low-voltage buses to meet the safety requirements of today's electric/hybrid vehicles. ▼ Figure 3: VOMA617A control cir- cuit schematic (Source: Vishay) Figure 2: Simplified schematic of the power stage (Source: Vishay)

Articles in this issue

Links on this page

view archives of Supplier eBooks - Vishay - An Automotive Grade Above