Supplier eBooks

Vishay - An Automotive Grade Above

Issue link: https://resources.mouser.com/i/1429079

Contents of this Issue

Navigation

Page 16 of 27

mouser.com/vishay / 17 Learn More VEML6031X00 Ambient Light Sensors Figure 5: Ambient light sensors can be implemented for display dimming at night. (Source: Vishay) Display Dimming While the proximity sensors gather information about what is happening in front of the display, Vishay's AEC-Q101-qualified VEML6031X0 ambient light sensor (ALS) can be implemented for display dimming (Figure 5). The main challenge faced in these applications is the increasingly dark cover materials used in automotive interiors, at times allowing less than 1 percent of visible light to pass through. This requires a sensor with very high sensitivity (down to 0.0023lx/count) so that even very low light conditions can be sensed and reacted to accordingly. To account for the increase of dark current with regard to temperature fluctuations, the part features active temperature compensation to make sure that the read lux value always stays within range. The robust 6-pin automotive package allows for stability across a high-temperature range and features opaque side walls so that stray light does not affect the results. Because the sensitivity is trimmed within the package, it results in a low part- to-part tolerance, reducing the complexity of calibration in the end design. To test all of these features, Vishay offers a complete support package with every sensor, including a dedicated application note and demo board, and demonstration software to get up and running quickly. Ray simulation files and C/C++ libraries are also offered so that application-based optical and mechanical implementations can be simulated and prototypes can be set up easily. ▼

Articles in this issue

Links on this page

view archives of Supplier eBooks - Vishay - An Automotive Grade Above