Supplier eBooks

Vishay - An Automotive Grade Above

Issue link: https://resources.mouser.com/i/1429079

Contents of this Issue

Navigation

Page 22 of 27

mouser.com/vishay / 23 X1 X3 TR1 SQC60002E TR2 SQC60002E R1 50uR R2 10R/10W GATE_PRELOAD NTC2+ NTC2- NTC2 NTC 10k GATE_MAIN2 SOURCE_MAIN2 V-IN+ V-OUT+ SENSE- SENSE+ SOURCE_PRELOAD GATE_MAIN1 SOURCE_MAIN1 NTC1+ NTC1- NTC1 NTC 10k TR3 SQSA80ENW X1 X3 TR1 SQC60002E TR2 SQC60002E R1 50uR R2 10R/10W GATE_PRELOAD NTC2+ NTC2- NTC2 NTC 10k GATE_MAIN2 SOURCE_MAIN2 V-IN+ V-OUT+ SENSE- SENSE+ SOURCE_PRELOAD GATE_MAIN1 SOURCE_MAIN1 NTC1+ NTC1- NTC1 NTC 10k TR3 SQSA80ENW Learn More Learn More NTCS SMD NTC Thermistors SQSA80ENW TrenchFET ® power MOSFETs Figure 3: Simplified schematic of the ICSS power stage (Source: Vishay) (10ms), and the output voltage X3 (in Figure 3) is monitored. If the output voltage has not reached ~90 percent of the input voltage after that time, the process is terminated, with the assumption a short circuit has occurred in the load or wiring. If the output has reached the appropriate level, then TR3 is switched off, and TR1/TR2 is switched on to energize the load. With regard to protection features, a Vishay NTCC300E4 wire bondable thermistor (NTC1 in Figure 3) is used to monitor the MOSFET die temperatures. Using wirebondable NTCs ensures very close proximity to the MOSFET junction temperature, the crucial measurement point. In the case of an over-temperature condition, the load is disconnected from the battery. The control circuitry is monitored for temperature overloads and a Vishay NTCS surface-mount thermistor (NTC2 in Figure 3). The load current is continuously monitored for battery health and overcurrent conditions using a customized version of a Vishay WSB8518-34 current shunt (R1 in Figure 3), which has a very low TCR (down to +-10 ppm/°C) and inductance which maximizes the accuracy of the output signal. A new high-current measurement and safety switch has been presented that can be used in any 12V or 48V battery management system as well as to control any high current load in the vehicle. ▼ Figure 2: ICSS power stage (Source: Vishay)

Articles in this issue

Links on this page

view archives of Supplier eBooks - Vishay - An Automotive Grade Above